9.6.7.11 Sizeof Built-in Function
The
SIZEOF(section)
built-in function
return the size in bytes of the named section, if that section has been allocated. If the
section has not been allocated when this is evaluated, the linker will report an error. In the
following example, symbol_1
and symbol_2
are assigned identical
values:SECTIONS{ ...
.output {
.start = . ;
...
.end = . ;
}
symbol_1 = .end - .start ;
symbol_2 = SIZEOF(.output);
...
}