6.2.3 B
Backward ref to unknown label label:
The referenced label is either not seen or not defined here.
Bad .common segment name.
Could not determine an appropriate alignment value for a .comm symbol. A previously seen .comm symbol may be incorrect.
Bad escaped character in string.
The string uses a non-standard backslash-escaped character.
Bad expression.
The expression type cannot be determined or an operand is not of the correct type for the expression type.
Bad floating literal: %s.
The token could not be converted to a floating-point value.
Bad floating-point constant: exponent overflow.
The token could not be converted to a floating-point value because of exponent overflow.
Bad floating-point constant: unknown error code=%d.
The token could not be converted to a floating-point value.
Bad format for ifc or ifnc.
The arguments to the ifc or ifnc directive are incorrect. They must be 2 comma-separated, double-quoted strings.
Bad or irreducible absolute expression.
The absolute expression had an unexpected operator type.
Bad register expression.
The DWARF debugging directive has an invalid register expression.
Bignum invalid.
The bignum value specified in the expression is not valid.