6.2.9 I
Ignoring attempt to redefine symbol name.
The symbol being redefined by the .weakext directive has already been defined.
Improper insert size.
The width of the field specified to an INS instruction was not valid for the shift position.
Improper extract size.
The width of the field specified to an EXT instruction was not valid for the shift position.
Instruction insn requires absolute expression.
This instruction requires a constant expression.
Invalid astatic register list.
The aregs field of a MIPS32e extended SAVE/RESTORE instruction specified an invalid astatic register list.
Invalid arg register list.
The aregs field of a MIPS32e extended SAVE/RESTORE instruction specified an invalid arg register list.
Invalid coprocessor 0 register number.
An invalid coprocessor 0 register number was passed to this instruction.
Invalid coprocessor sub-selection value (%ld), not in range 0-7.
The coprocessor sub-selection value must be in the range 0-7.
Invalid frame size.
The frame size is not valid and could not be encoded.
Invalid identifier for .ifdef.
The specified identifier is not a valid name. It must begin with a legal character.
Invalid register list.
In MIPS32 mode, the register list contained an invalid register.
Invalid segment %s.
Attempting to change the location counter in an invalid segment.
Invalid static register list.
The static register list should include only $s2-$s8