6.2.6 E
End of file inside conditional.
The assembler identified a missing conditional-end directive. Terminate the conditional before the end of the file.
End of macro inside conditional.
The assembler identified a missing macro-end directive. Terminate the macro before the end of the file.
Expected address expression.
The expression was illegal, absent, or bignum but it should have been a constant address.
Expected comma after %s.
The arguments for this directive must be separated by a comma.
Expected comma after name `%s' in .size directive.
The arguments for this directive must be separated by a comma.
Expected quoted string.
The argument should be a quoted string.
Expected simple number.
This argument must be a simple number.
Expected symbol name.
This argument must be a symbol name.
Expression out of range.
The expression is out of range for the directive or instruction (e.g. 32-bit value when a 32-bit value is expected)
Expression too complex.
The expression should be a symbol or constant.