6.3.14 U
Unknown escape \escape in string; ignored.
The string contains an unrecognized backslash-escaped character. Check that the character following the backslash is correct.
Used $at without .set noat.
This code is using the $at (assembler temporary) register, but the
assembler may use it when generating synthesized macro instruction. Use the .set noat directive to tell the assembler not to quietly use
this register.