3.22 __regvar Keyword
The IAR __regvar keyword places static storage duration variables in registers
or register sets.
Suggested Replacement
There is an MPLAB XC8 feature that performs a similar tasks to this keyword, but there are some differences in its effect.
Use the asm("reg") syntax along with the standard
register keyword when defining an object to place that object
in a register or in consecutive
registers. Note that the compiler will issue an error if an attempt is made to reserve critical registers (like argument registers or the frame pointer register) using this option.
Caveats
The compiler might use the registers assign in different translation units.
Examples
__regvar __no_init int myVar @ 14;
volatile int x;
int main() {
x = myVar;
}and
the --lock_regs 2IAR compiler option to MPLAB XC8 code similar
to:register int myVar asm("r14");
volatile int x;
int main() {
x = myVar;
}Further Information
See the Register Usage and Variables in Registers section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on writing interrupt functions.