3.18 __no_init Keyword
The IAR __no_init keyword specifies that the qualified object is not initialized
by the runtime startup code.
Suggested Replacement
There is a MPLAB XC8 specifier that performs a similar task.
Use the __persistent specifier or (or its expanded form,
__attribute__((persistent)) with the object's definition.
Caveats
The Common C Interface must be enabled using -mext=cci to use the
__persistent specifier form.
Examples
volatile __no_init int x;
int main(void) {
x = 2;
return 0;
}to
MPLAB XC8 codes similar
to:#include <xc.h>
volatile __persistent int x;
int main(void) {
x = 2;
return 0;
}Further Information
See the Attributes and Options for Controlling the C Dialect sections in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on this option and attribute.