3.9 __hugeflash Keyword
The IAR __hugeflash keyword places and accesses objects in huge program memory
(addressable range 0x0-0x7FFFFF). Pointer arithmetic and access is all 24-bit. Pointers
qualified with this keyword can point to any address in this range.
Suggested Replacement
There are two ways of having MPLAB XC8 code perform a similar task to this keyword.
When the -mconst-data-in-progmem const-in-program-memory feature is
in effect (the default operation), this IAR keyword can simply be removed. In this
case, all const-qualified objects are automatically placed in and
read from program memory, and 24-bit wide pointers are used.
When the -mno-const-data-in-progmem option has been used to disabled
the const-in-program-memory feature, use the MPLAB XC8 __memx
qualifier, which places const objects in flash and accesses these
using 24-bit addresses.
Caveats
The const qualifier must be used with the __memx
qualifier when using MPLAB XC8, whereas this is only preferable when using
__hugeflash with IAR.
Access of objects using __memx will be slightly slower than those
using a 24-bit flash-only pointer, as __memx addresses represent a
combined flash + data memory address space.
Examples
__hugeflash char arr[] = "abc";
volatile int x;
int main(void) {
x = arr[x];
}to
MPLAB XC8 code similar
to:#include <xc.h>
const char arr[] = "abc";
volatile int x;
int main(void) {
x = arr[x];
}when
the -mno-const-data-in-progmem const-in-program-memory feature is
enabled, or
to:#include <xc.h>
const __memx char arr[] = "abc";
volatile int x;
int main(void) {
x = arr[x];
}
when the const-in-program-memory feature has been disabled.Further Information
See the Special Type Qualifiers and Options Specific to AVR Devices sections in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on this qualifier and option.