3.7 __generic Keyword
The IAR __generic keyword is used with pointer definitions to allow those
pointers to accesses objects from both data and program spaces, based on the MSb of the
address. The pointer size varies with the selected device.
Suggested Replacement
There are MPLAB XC8 qualifiers that performs similar tasks to this keyword, but there are some differences in their effect.
If the const-in-program-memory feature is enabled (the default state), use the
standard const qualifier provided by MPLAB XC8 with a pointer
definition on devices which do not map their program memory in the data space to
make that pointer 24-bits wide.
If this feature is disabled, using the -mno-const-data-in-progmem
option, use both the const and __memx qualifiers
with a pointer definition. In either case, the MSb of the pointer's address is used
to determine whether to read from the data or program address spaces. Such pointers
can access the lower 64 KB of the data space.
Caveats
If the const-in-program-memory feature is disabled, alternate versions of the string
functions normally provided by <string.h> must be used to
access string objects located in program memory.
Examples
const __generic char * p;
volatile char x;
int main(void) {
x = *p;
}to
MPLAB XC8 code similar
to:#include <xc.h>
const __memx char * p;
volatile char x;
int main(void) {
x = *p;
}
Further Information
See the Special Type Qualifiers and Options Specific to AVR Devices sections in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on this qualifier and option.