3.2 __ext_io Keyword
The IAR __ext_io keyword specifies that the qualified object aliases
memory-mapped SFRs, that is, the object is accessed from the AVR's IO registers. This is
similar to the IAR __io attribute, except that it is meant for
accessing SFRs above addresses 0x100.
Suggested Replacement
There is an MPLAB XC8 attributes that performs a similar tasks to this keyword, but there are some differences in its effect.
The MPLAB XC8 address attribute equates a symbol to an address,
permitting the symbol to represent a register in the I/O space.
Caveats
The IAR __ext_io keyword ensures that memory is allocated to the
object. That memory will be in the I/O space. When using the MPLAB XC8
address attribute, the compiler does not assign memory to the
symbol; instead, it assumes that the symbol represents a peripheral register and
merely equates the symbol to an address, which must be specified in the
attribute.
Use of __ext_io implies the object is volatile.
This is not the case when using the MPLAB XC8 address
attribute.
Examples
__ext_io char TCB0_CTRLA;
int main(void) {
volatile char x = TCB0_CTRLA;
}to
MPLAB XC8 code similar
to:volatile char TCB0_CTRLA __attribute__((address(0xB00)));
int main(void) {
volatile char x = TCB0_CTRLA;
}
In this example, the compiler does not allocate memory at 0xB00; it merely assigns
that address to the TCB0_CTRLA identifier.Further Information
See the Attributes section in the MPLAB XC8 C Compiler User's Guide for AVR MCUs for more information on this attribute.