6.6.1.6 Zigbee Application Demo: Multi-Sensor with Low Power Functionality

WBZ351 Curiosity Board

Devices (Device): | PIC32CX5109BZ31048(MCU) on WBZ351 module |

Peripherals (Used, On-Board): | UART-USB Converter|

Introduction

This tutorial will help users to create a low power enabled multi-sensor end device application which can get connected with a Combined Interface(CI) and report the sensor values.

GitHub Repository

The firmware, .hex, and accompanying readme.md file for the application can be found in the GitHub repository – multisensor

Hardware Requirement

Table 6-19. Hardware Prerequisites
S. No. Tool Quantity
1WBZ351 Curiosity Boards2
2Micro USB cable2
3Personal Computer1

SDK Setup

Refer to Getting Started with Software Development from Related Links.

Software Requirement

To install Tera Term tool, refer to the Tera Term web page in Reference Documentation from Related Links.

Programming the Precompiled Hex File or Application Example

The Multi-Sensor is an end device application. The Multi-Sensor application works by getting connected with a co-ordinator device(Combined Interface). So, to successfully execute this demo, it is mandatory to have a combined interface application set up prior to running the multi-sensor application.

  1. First program the WBZ351Curiosity board with Combined Interface which can act as Zigbee Gateway/Coordinator. The details regarding the combined interface application including programing steps is provided Refer to the combined Interface application (Reference section). Gather the information regarding the combined interface application, and program the application to one of the curiosity board.

  2. Program another WBZ351 Curiosity board with Multi-Sensor application. Follow the steps mentioned below to program the curiosity board with Multi-Sensor application.

Using MPLAB® X IPE:

  1. Import and program the precompiled hex file: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\zigbee\multisensor.

  2. For detailed steps, refer to Programming a Device in MPLAB® IPE in Reference Documentation from Related Links.
    Note: Ensure to choose the correct Device and Tool information.

Using MPLAB® X IDE:

Follow the steps below to run a precompiled application example.

Prerequisites:

  1. Install MPLAB X IDE

  2. Install XC32 Compiler

  3. Install Device Family Part Pack

  4. Install MCC Plugin

  5. Install Harmony 3 Dependencies

Open, Build and Program an existing application example:

  1. Connect Curiosity Board to the PC using usb cable

  2. Open MPLAB X IDE

  3. Select File > Open Project

  4. Browse to project location: <Discover Path>\wireless_apps_pic32cxbz3_wbz35\apps\zigbee\multisensor\\firmwareInformation related to the workings of the application example are available in readme.md file available in the multi-sensor folder
  5. Open Project Properties

    • Select WBZ351 Curiosity Board as hardware tool for programming

    • Ensure correct DFP is selected as mentioned in the Tools and Harmony Components

  6. Select XC32 compiler

  7. Select option Build Project in IDE to compile the application example

  8. Select option Run Project in IDE to program the target – the onboard debugger will program the example application

For more details on how to find the Discover path, refer to Download Application Example from Discover in Running a Precompiled Application Example from Related Links.

Demo Description

This application demonstrate the working of Zigbee Multi-Sensor end device joining to Zigbee Coordinator (Combined Interface) . After joining, multi-sensor device will start ZCL attribute reporting of sensor data such as temperature, occupancy, light, and humidity.

Application Zigbee Logical Device Type Functionality
Combined InterfaceCoordinatorDevice capable of controlling and monitoring other devices. It is typically a mains-powered device like a personal computer
Multi-SensorEnd DeviceReports sensor data such as temperature, occupancy, light, and humidity periodically to gateway

The application demonstration required to have a combined interface application up and running in the vicinity. which can act as Zigbee Gateway/Coordinator. The Multi-Sensor application here can act as Zigbee end device.

Commissioning.

The Zigbee Multi-Sensor can be connected to a zigbee network.

Joining Multi-Sensor with WBZ351Combined Interface (CI) Coordinator

# Hardware & Software Setup

  1. Supply power to WBZ351 Curiosity Board consisting of Combined Interface application by connecting a USB cable.

  2. The application activity is shown as “Console Log” through on-board UART-USB converter
    • Open Terminal(Example: Tera Term) with the setup as shown below to see the log
    • On the PC side virtual COM port connection that corresponds to the board shall have following settings:
      • BAUD RATE: 115200 (as configured in SERCOM configuration)
      • PARITY: None
      • DATA BITS: 8
      • STOP BITS: 1
      • FLOW CONTROL: None
      Additionally, local echo and sending line ends with line feeds shall be enabled in the PC serial terminal application.
  3. Make the serial terminal ready and then press the reset button on the curiosity board. Below log will be displayed.

# Network Formation (Coordinator - (Combined Interface))

  1. Once the board is powered on and serial terminal setup is done, the board is ready to be operated as a coordinator. It is responsible for initially forming the network and then, via the Trust Centre functionality, managing which other devices are allowed to join the network and distributing security keys to those that are allowed to join.

  2. Input command : resetToFN and look for the below logs for successful zigbee network formation on CI. It will open up the network for other zigbee devices to join for first 180 seconds from the first power ON.

  • Case1: If a near by device is trying to join a network, and sees CI then will join the network as shown in below log.
  • Case 2: The commissioning procedure will last for 180 seconds. In case no other devices are there in vicinity and at the end of 180 seconds, the below log will be displayed
  • Case 3: To open up the network after 180 seconds to allow other devices to join, we have to input the below commands in CI, before commissioning is initiated in another device.

    setPermitJoin 180→ This command opens up the network for next 180 seconds

    invokeCommissioning 8 0 → This command opens up the network for “finding and binding procedure”

# Commissioning (End Device - Multi-Sensor)

  1. Supply power to WBZ351 Curiosity Board which is programmed with Multi-Sensor image by connecting a USB cable. The Multi-Sensor will search for Zigbee coordinator device and will join to network and initiate Finding & Binding.
  2. Once Multi-Sensor finishes Finding & Binding procedure, it will start attribute reporting. The Combined interface terminal log will print the received attribute information as shown below.

Developing this Application from scratch using MPLAB Code Configurator

Follow the steps below to build the application manually:
Note: It is recommended for the new users of the MPLAB Code Configurator to refer MPLAB® Code Configurator (MCC) User’s Guide in Reference Documentation from Related Links.
  1. Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.

  2. Add “Multi-Sensor” device type to the project and accept all the dependencies

    Accept all the component auto-activation and attachment auto-connect confirmation.

    Confirm “Yes” for the Attachment Auto-Connect requests

  3. After the inclusion of the dependent components, the final project graph looks like.

  4. System Clock Configuration and SOSC selection during Sleep mode

    System Clock Selection

    SOSC Clock Configuration

    Note: Even after enabling and selecting the SOSC as backup source in the clock configuration. The LPCLK and RTC clock still show as 0Hz. This is a known issue which will be resolved in upcoming MCC release. For the time being, to fix this issue, a manual application code modification is necessary. The required change will be discussed in the next section.
  5. Generate Code

    Now all the required components has been added to the project and necessary configuration modification is made. The next step is to generate the application code.

Manual Application code edit

This section talks about the mandatory code modifications that needs to be incorporated inorder to implement the sleep mode functionality.

Step 1: app_user_edits.c

  • Some of the Harmony 3 generated files cannot be fully configured by the MPLABX Code Configurator. This file contains the instructions for the user to modify these files.

    Follow the instruction mentioned on the app_user_edits.c file and after completing the required edits, comment out or remove the #error line

Step 2: plib_gpio.c

  • Code Changes for Sleep functionality

    Add the below code inside the GPIO_Intitialize function

    These changes are made to set the default states of respective GPIO pins in consideration to save the power.

    void GPIO_Initialize ( void )
    {
     /* Disable JTAG since at least one of its pins is configured for Non-JTAG function */
        CFG_REGS->CFG_CFGCON0CLR = CFG_CFGCON0_JTAGEN_Msk;    
    //All pubs are defined as input after a reset.
        GPIOA_REGS->GPIO_TRISSET = 0xFFFF; //Set all pins as input
        GPIOA_REGS->GPIO_CNPUSET = 0x7FF3; //Except PA2 (QSPI Data), PA3, the others are pulled up
        GPIOA_REGS->GPIO_CNPDSET = 0x0008; //RPA3 is Pulled down: SERCOM 0-RTS
        /*  PB  */
        GPIOB_REGS->GPIO_ANSELSET = 0x0040; //PB6 ANSEL for Temp sensor
        GPIOB_REGS->GPIO_TRISSET = 0xFFFF;  //Set all pins as input
        GPIOB_REGS->GPIO_CNPUSET = 0x3D96;  //Pull up: PRB 1, 2, 4, 7, 8, 10, 11, 12 , 13
        GPIOB_REGS->GPIO_CNPDSET = 0x0029;  //Pull down RB0,3,5 for LED
              /* PORTA Initialization */
        /* PORTB Initialization */
        /* PPS Input Remapping */
        /* PPS Output Remapping */
    }
    
  • Step 3:Step 4 - Plib_rtc.h

    • Default Generated: #define RTC_COUNTER_CLOCK_FREQUENCY (0U / (1UL << (0x1U - 1U)))
    • Replace to: #define RTC_COUNTER_CLOCK_FREQUENCY (32768U / (1UL << (0x1U - 1U)))

      Note:This particular change is made to compensate the known issue earlier discussed in clock configuration. This issue will be resolved in the upcoming release and the MCC auto generated code will have the required change by default.

  • Step 4: zigbeeAppDeviceSelect.h

    • Default Generated: #define CS_UID 0xbee //Unique Identifier (UID) determining the device extended address
    • Change to a unique value: #define CS_UID 0x123bee //Unique Identifier (UID) determining the device extended address

    Reason:By default the Co-ordinator is also having same value. In a network the UID value should be unique

Related Information:

Zigbee Centralized Network Formation by Combined Interface