ZCL_StartSecurityReq Function
C
void ZCL_StartSecurityReq(ZCL_StartSecurityReq_t *req);Description
Initializes the KE cluster, discovers KE devices and performs key establishment
The function should be called in applications supporting the Key Establishment (KE) cluster, to perform key establishment procedures. The behavior is different on the trust center and common devices.
On the trust center:
If the \c remoteAddress field is set to 0, KE cluster will be initialized.
Key establishment will not be performed with any device.
If \c remoteAddress is set to the extended address of a remote device the
trust center will start key establishment with it.
On a common device:
If the \c remoteAddress field is set to 0 or to the extended address of the
trust center, the key establishment with the trust center will start.
Otherwise, the request will eventually fail.
If Certicom Security is not used, the success status is always reported.
Response statuses: Accessed via the ZCL_StartSecurityConf_t-status field of the ZCL_StartSecurityReq_t-ZCL_StartSecurityConf callback's argument.
All possible status codes are wrapped in the -ZCL_SecurityStatus_t enumeration.
Parameters
| Param | Description |
|---|---|
| req | request structure to pass attribute id |
Returns
None