1.4.3.10 _LIBQ_Q16Sqrt Function
Square root of a positive _Q16 fixed point value.
Description
_Q16 _LIBQ_Q16Sqrt(_Q16 x);Calculate the square root of a positive _Q16 fixed point value, and return the _Q16 result.
Preconditions
The input value must be positive.
Parameters
x The _Q16 fixed point value input from which to find the square root.
Returns
_LIBQ_Q16Sqrt returns the _Q16 fixed point value which is the square root of the input parameter.
Remarks
Execution Time (cycles): 240 typical (104 to 258)
Program Memory 152 bytes
Error <= 0.000015258789 (accurate to least significant _Q16 bit)
Example
_Q16 squareRoot; squareRoot = _LIBQ_Q16Sqrt((_Q16)0x01000000); _// The square root of 256.0 is 16.0 (0x00100000)_ squareRoot = _LIBQ_Q16Sqrt((_Q16)0x00004000); _// The square root of 0.25 is 0.5 (0x00008000)_ squareRoot = _LIBQ_Q16Sqrt((_Q16)0x5851f42d); _// The square root of 22609.953125 is 150.366074_ _(0x00965db7)_
C
_Q16 _LIBQ_Q16Sqrt (_Q16 x );