1.4.4 LibQ Fixed-Point "C" Math Library
Introduction
This topic describes the LibQ Fixed-Point C Math Library.
Description
The LibQ Fixed-Point C Math Library is written in C and is available for all processors supported by Harmony 3.
The libq_c Fixed-Point Math Library provides fixed-point math functions written in C for portability between core processors. The library uses signed fixed point types (fractional Q types specified by Qn.m) which are specifed as follows in the library names:
Qndm where:
• n is the number of data bits to the left of the radix point
• m is the number of data bits to the right of the radix point
• a signed bit is implied (unless stated otherwise)
For convenience, short names are also defined for arbitrary scaled fractional types:
• q15 is signed fractional 16 bit value
• q31 is signed fractional 32 bit value
• i16 is signed integer, i.e. Q16d0
In addition, A pseudo floating point 32 bit format (FxQFloat32) is defined that consists of 16 mantissa and a 16 bit exponent (base 2). Functions in the library are prefixed with the type of the return value and followed by argument types (in order):
libq_<result><name><args>
For example, libq_q1d15_Sin_q10d6 returns a Q1.15 value equal to the to the sine of an angle specified as a Q10.6 value (in degrees between 0 and 360).
For arbitrary scaled types (q15, q16, q31, and q32) the scaling of the result will depend on the function and the scaling of the arguments. For instance, libq_q15_Add_q15_q15(a,b) will return a scaled value type that is the two input types (which must have equivalent scaled value type).
Configuring the Library using MCC
Select the Audio/Math/Math Libraries component to load the libq_c, libq/dsp libraries, as shown below.
The project configuration should now contain the Math Libraries block.
The configuration window (when the block is selected) looks like the following:
Remarks
The libq_c functions do not correspond to the libq fixed-point library optimized for the microaptive core processor and written in asm.
Library Overview
LIBQ_C math functions:
• Sine: libq_q1d15_Sin_q10d6, libq_q20d12_Sin_q20d12
• Abs: libq_q15_Abs_q15, libq_q31_Abs_q31
• Negate: libq_q15_Negate_q15, libq_q31_Negate_q31
• Round: libq_q15_RoundL_q31
• Deposit: libq_q31_DepositH_q15, libq_q31_DepositL_q15
• Extract: libq_q15_ExtractH_q31, libq_q15_ExtractL_q31
• Add: libq_q15_Add_q15_q15, libq_q31_Add_q31_q31
• Subtract: libq_q15_Sub_q15_q15, libq_q31_Sub_q31_q31
• Shift(Scale): libq_q15_ShiftLeft_q15_q15, libq_q31_ShiftLeft_q31_q15, libq_q15_ShiftRight_q15_q15, libq_q31_ShiftRight_q31_q15, libq_q15_ShiftRightRound_q15_q15, libq_q31_ShiftRightRound_q31_q15
• Multiply: libq_q15_Mult_q15_q15, libq_q15_MultipyR2_q15_q15, libq_q31_Multi_q15_q31
• Divide: libq_q15_DivisionWithSaturation_q15_q15
• Multiply-Accumulate: libq_q31_Mac_q31_q15_q15, libq_q15_MacR_q31_q15_q15
• Multiply-Subtract: libq_q31_Msu_q31_q15_q15, libq_q15_MsuR_q31_q15_q15
• Exponential-Averaging: libq_q15_ExpAvg_q15_q15_q1d15
LIBQ_C conversion functions:
• Normalize Q value: Fx16Norm, Fx32Norm
• Float-to-Q value: Fl2Fract16, Fl2Fract32, Fl2FxPnt16, Fl2FxPnt32, Fl2FxPnt
• Float-To-Integer: Fl2Int16, Fl2Int32
Library Interface
Functions
| Name | Description |
|---|---|
| CosInDegs | Calculates fixed point Cos(theta) (Q0.15 fixed point), where theta is in degrees (Q8.6 fixed point). |
| Fract_10toX_Q15bfp | Calculates pow(2,x) with fixed point math. |
| Fract_10toX_Q15bfpFromQ15d16 | Calculates pow(2,x) with fixed point math. |
| Fract_10toX_Q15d16 | Calculates pow(2,x) with fixed point math. |
| Fract_2toMinusX_Q15 | Calculates pow(2,-x) with fixed point math. |
| Fract_2toX_Q15bfp | Calculates pow(2,x) with fixed point math. |
| Fract_2toX_Q15bfpFromQ15d16 | Calculates pow(2,x) with fixed point math. |
| Fract_2toX_Q15d16 | Calculates pow(2,x) with fixed point math. |
| Fract_Convert_Q15bfpToQ15d16 | Convert Q15 block floating point to Q15.16 fixed point. |
| Fract_Convert_Q15bfpToQ31 | Convert Q15 block floating point to Q31 fixed point. |
| Fract_Convert_Q15d16ToQ15bfp | Convert from Q15.16 fixed point to Q15 Block Floating Point. |
| Fract_Convert_Q15ToQ15bfp | Convert from Q15 fixed point to Q15 Block Floating Point. |
| Fract_InversePower | Computes pow(nBase,-nExponent). |
| Fract_log10fix | Calculates fixed point base 10 logarithm using number of fractional bits specified by precision argument. |
| Fract_log2fix | Calculates fixed point base 2 logarithm using number of fractional bits specified by precision argument. |
| Fract_Power | Computes pow(nBase,nExponent) using for loop. |
| Fract_sqrtQ15 | Fixed point Q15 squareroot. |
| Fract_XminusY_Q15bfp | Subtract two Q15 block floating point numbers. |
| Fract_XoverY_Q15bfp | Division x/y as Q15 block floating point. |
| Fract_XoverY_Q15bfpFromQ15 | Calculate ratio of X/Y as Q15s but return result as Q15 block floating point. |
| Fract_XoverY_Q15d16FromQ15 | Calculates ratio X/Y for two Q15 fixed points. |
| Fract_XplusY_Q15bfp | Add two Q15 block floating point numbers. |
| Fract_XtimesY_Q15 | Calculates product of X*Y for Q15 fixed point. |
| Fract_XtimesY_Q15bfp | Multiply X times Y, for Q15 block floating point arguments. |
| Fract_XtimesY_Q15d16 | Calculates product of X*Y for Q15.16 fixed point. |
| Fract_XtimesY_Q31 | Calculates product of X*Y for Q31 fixed point. |
| Fx16Norm | Normalize the 16-bit fractional value. |
| Fx32Norm | Normalize the 32-bit number. |
| libq_q15_Abs_q15 | Saturated Absolute value. |
| libq_q15_Add_q15_q15 | Add two 16-bit 2s-complement fractional values. |
| libq_q15_DivisionWithSaturation_q15_q15 | Fractional division with saturation. |
| libq_q15_ExpAvg_q15_q15_q1d15 | Exponential averaging. |
| libq_q15_ExtractH_q31 | Extracts upper 16 bits of input 32-bit fractional value. |
| libq_q15_ExtractL_q31 | Extracts lower 16-bits of input 32-bit fractional value. |
| libq_q15_MacR_q31_q15_q15 | Multiply accumulate with rounding. |
| libq_q15_MsuR_q31_q15_q15 | Multiply-Subtraction with rounding. |
| libq_q15_MultiplyR2_q15_q15 | Fractional multiplication of two 16-bit fractional values giving a 16 bit rounded result. |
| libq_q15_Negate_q15 | Negate 16-bit 2s-complement fractional value with saturation. |
| libq_q15_RoundL_q31 | Rounds the lower 16-bits of the 32-bit fractional input. |
| libq_q15_ShiftLeft_q15_i16 | Arithmetic Shift of the 16-bit input argument. |
| libq_q15_ShiftRight_q15_i16 | Arithmetic RIGHT Shift on a 16-bit value. |
| libq_q15_ShiftRightR_q15_i16 | Performs an Arithmetic RIGHT Shift on a 16-bit input. |
| libq_q15_Sub_q15_q15 | Subtract two 16-bit 2s-complement fractional values. |
| libq_q1d15_Sin_q10d6 | Approximates the sine of an angle. |
| libq_q20d12_Sin_q20d12 | 3rd order Polynomial apprx. of a sine function. |
| libq_q31_Abs_q31 | Saturated Absolute value. |
| libq_q31_Add_q31_q31 | Add two 32-bit 2s-complement fractional values. |
| libq_q31_DepositH_q15 | Place 16 bits in the upper half of 32 bit word. |
| libq_q31_DepositL_q15 | Place 16 bits in the lower half of 32 bit word. |
| libq_q31_Mac_q31_q15_q15 | Multiply-Accumulate function WITH saturation. |
| libq_q31_Msu_q31_q15_q15 | L_msu(a,b,c) |
| libq_q31_Mult2_q15_q15 | Fractional multiplication of two 16-bit fractional values. |
| libq_q31_Multi_q15_q31 | Implement 16 bit by 32 bit multiply. |
| libq_q31_Negate_q31 | Negate 32-bit 2s-complement fractional value with saturation. |
| libq_q31_ShiftLeft_q31_i16 | Arithmetic Shift of the 32-bit value. |
| libq_q31_ShiftRight_q31_i16 | Arithmetic RIGHT Shift on a 32-bit value. |
| libq_q31_ShiftRightR_q31_i16 | Arithmetic RIGHT Shift on a 32-bit value |
| libq_q31_Sub_q31_q31 | Subtract two 32-bit 2s-complement fractional values |
| LUTwInterpolation_Q15 | Calculates calculates y = f(x) based on a lookup table with linear interpolation between table entries. |
| SinInDegs | Calculates fixed point Sin(theta) (Q0.15 fixed point), where theta is in degrees (Q8.6 fixed point) |