1.4.3.24 _LIBQ_Q31FromFloat Function
Converts a float to a _Q31 value.
Description
_Q31 _LIBQ_Q31FromFloat(float x);Converts a floating point value to a _Q31 fixed point representation. The _Q31 fixed point value is returned by the function. The conversion will saturate if the value is outside the range of the _Q31 representation.
Preconditions
None.
Parameters
x The floating point value to convert to _Q31 fixed point.
Returns
_LIBQ_Q31FromFloat returns the _Q31 fixed point value corresponding to the floating point (float) input value.
Remarks
The C library functions __gesf2, __lesf2, __addsf3, __mulsf3, and __fixsfsi are called by this routine and thus must be linked into the executable image.
Execution Time (cycles): 210 typical (158 to 214)
Program Memory 100 bytes
Example
_Q31 q31; q31 = _LIBQ_Q31FromFloat(( float )0.000008); _// q31 now equals (_Q31)0x00004000_ q31 = _LIBQ_Q31FromFloat(( float )-1.0); _// q31 now equals (_Q31)0x80000000_ q31 = _LIBQ_Q31FromFloat(( float )0.690001); _// q31 now equals (_Q31)0x5851f400_
C
_Q31 _LIBQ_Q31FromFloat ( float x );