The following table provides the command syntax for Gain mode settings.
Table 3-4. Gain Mode setting: After Initialization, Before TX Start
Command Syntax
MCHPRT 11 X
X
X refers to Gain mode:
0 – Dynamic gain mode
1 – Bypass gain mode (default)
2 – Flash gain mode
Example
MCHPRT 11 1
Bypass mode
The following figure shows the example of Gain mode.Figure 3-6. Console Log of Gain Mode
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.