The following table provides the command syntax for Antenna switch (ATWILC1000/ATWINC15X0).
Table 3-5. Antenna Switching: After Initialization
Command Syntax
MCHPRT 12 X Y
X
X refers to Antenna:
0 – antenna 1 (default)
1 – antenna 2
Y
Y refers to GPIO pin:
3 – GPIO3
Example
MCHPRT 12 0 3
Antenna switching A
The following figure shows the example of Antenna switch.Figure 3-7. Console Log of Antenna Switch
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.