1.7 PCS Rate Switch Between 8b10b and 64b66b Mode for CPRI
(Ask a Question)All CPRI protocol data rates are statically supported with the Libero Transceiver Configurator using either 8b10b or 64b66b modes. 8b10b supports CPRI rates 2, 3, 4, 5, 6, and 7 while 64b66b mode supports rates 7a, 8, and 9. In cases requiring dynamic switching, the user must take steps to accommodate the correct design intentions for switching the PCS mode between the data rates. This case requires a rate switch between the 8b10b and 64b66b modes.
8b10b ports are a superset of 64b66b ports. This implies that the user must plan the FPGA fabric design to interface with 8b10b ports of the XCVR and use the fabric to control the mode switching to the CPRI user IP as shown in the following figure.
The following table lists the port crossover between the 8b10b and 64b66b modes provided by the XCVR PCS to the FPGA fabric.
| Direction | 8B10B Mode | 64B6xB Mode |
|---|---|---|
| Input | TX_DISPFNC[15] | TX_ELEC_IDLE |
| Input | TX_DISPFNC[14] | TX_BYPASS_DATA |
| Input | TX_DISPFNC[13:12] | RESERVED_IN[1:0] |
| Input | TX_DISPFNC[11:8] | RESERVED_IN[5:2] |
| Input | TX_DISPFNC[7:6] | RESERVED_IN[7:6] |
| Input | TX_DISPFNC[5:2] | RESERVED_IN[11:8] |
| Input | TX_DISPFNC[1] | RESERVED_IN[12] |
| Input | TX_DISPFNC[0] | RESERVED_IN[13] |
| Input | TX_K[7:6] | RESERVED_IN[15:14] |
| Input | TX_K[5] | RESERVED_IN[16] |
| Input | TX_K[4] | TX_SOS |
| Input | TX_K[3:0] | TX_HDR[3:0] |
| Input | TX_DATA[63:33] | TX_DATA[63:33] |
| Input | TX_DATA[32:19] | TX_DATA[32:19] |
| Input | TX_DATA[18:17] | TX_DATA[18:17] |
| Input | TX_DATA[16] | TX_DATA[16] |
| Input | TX_DATA[15] | TX_DATA[15] |
| Input | TX_DATA[14] | TX_DATA[14] |
| Input | TX_DATA[13:12] | TX_DATA[13:12] |
| Input | TX_DATA[11:10] | TX_DATA[11:10] |
| Input | TX_DATA[9:8] | TX_DATA[9:8] |
| Input | TX_DATA[7:5] | TX_DATA[7:5] |
| Input | TX_DATA[4] | TX_DATA[4] |
| Input | TX_DATA[3] | TX_DATA[3] |
| Input | TX_DATA[2] | TX_DATA[2] |
| Input | TX_DATA[1] | TX_DATA[1] |
| Input | TX_DATA[0] | TX_DATA[0] |
| Output | RX_K[7] | RX_BYPASS_DATA |
| Output | RX_K[6:0] | RESERVED_OUT[6:0] |
| Output | RX_CODE_VIOLATION_7 | RESERVED_OUT[13:7] |
| RX_DISPARITY_ERROR_7 | ||
| RX_CODE_VIOLATION_6 | ||
| RX_DISPARITY_ERROR_6 | ||
| RX_CODE_VIOLATION_5 | ||
| RX_DISPARITY_ERROR_5 | ||
| RX_CODE_VIOLATION_4 | ||
| Output | RX_DISPARITY_ERROR_4 | RX_HDR_VAL |
| Output | RX_CODE_VIOLATION_3 | STATUS_HI_BER |
| Output | RX_DISPARITY_ERROR_3 | STATUS_LOCK |
| Output | RX_CODE_VIOLATION_2 | RX_SOS |
| Output | RX_DISPARITY_ERROR_2 | RX_DATA_VAL |
| Output | RX_CODE_VIOLATION_1 | RX_HDR[3:0] |
| RX_DISPARITY_ERROR_1 | ||
| RX_CODE_VIOLATION_0 | ||
| RX_DISPARITY_ERROR_0 | ||
| Output | RX_DATA[63:51] | RX_DATA[63:51] |
| Output | RX_DATA[50:49] | RX_DATA[50:49] |
| Output | RX_DATA[48:9] | RX_DATA[48:9] |
| Output | RX_DATA[8:5] | RX_DATA[8:5] |
| Output | RX_DATA[4] | RX_DATA[4] |
| Output | RX_DATA[3:1] | RX_DATA[3:1] |
| Output | RX_DATA[0] | RX_DATA[0] |
| Input | TX_BIT_CLK4 | |
| Input | TX_PLL_LOCK4 | |
| Input | TX_PLL_REF_CLK4 | |
| Input | CTRL_CLK5 | |
| Input | CTRL_ARST_N5 | |
| Input | CALIB_REQ5 | |
| Input | LOS5 | |
| Input | CDR_REF_CLK | |
| Output | CALIBRATING | |
| Input | TX_WCLK6 | |
| Input | PCS_ARST_N | |
| Input | PMA_ARST_N | |
| Output | RX_VAL | |
| Output | RX_READY | |
| Output | RX_IDLE | |
| Output | TX_CLK_STABLE | |
| Output | RX_CLK_[R:G] | |
| Output | TX_CLK_[R:G] | |
| Input | RXD_P | |
| Input | RXD_N | |
| Output | TXD_P | |
| Output | TXD_N | |
- Port names in Libero has prefix lane#_ appended to name.
- Refer to specific PCS port list tables for port description.
- Ports prefixed by RESERVED for a specific mode is not used for the MODE.
- Port is included in CLKS_FROM_TXPLL BIF.
- Port is included with Enhanced Receiver Management (ERM).
- TX_WCLK is included when Global (Shared) TX Clock is used.
The user control logic must accommodate switching transceiver control registers listed in the following table. This is typically by modifying the registers using the DRI to the transceiver from an APB within the design.
The following table outlines the affected registers that must be modified during rate switching.
| Register Page xls | Register Name | Field Name | Description | Required Value for 8B10B | Required Value for 64B6xB |
|---|---|---|---|---|---|
| pcslane | L8_R0 | L8_TXENCSWAPSEL | Selects between 1000BASE-X/T and Fibre Channel octet-swapping modes. | Optional: 0=1000BASE-X/T, 1=Fibre Channel | Don’t-care |
| L8_GEARMODE[1:0] | Sets data path width of FWF interfaces. | Must be consistent with clock selections for txfwf_rclk and rxfwf_wclk. | Don’t-care | ||
| LOVR_R0 | FAB_IFC_MODE[3:0] | Selects path through fabric and FWF overlay blocks. | Register changes the
meanings of the epcs_tx_data and epcs_rx_data pins based on the setting
of the pcslane LOVR_R0:PCSPMA_IFC_MODE[3:0] control register field. The PCSPMA_IFC_MODE is one-hot encoded as follows: 0b0100 == 8B10B mode | PCSPMA_IFC_MODE is one-hot
encoded as follows 0b0010 == 64B6xB mode | |
| PCSPMA_IFC_MODE[3:0] | Selects lane mode for driving data into the SerDes serializer. | ||||
| LCLK_R0 | LCLK_EPCS_RX_CLK_SEL [1:0] | Chooses which clock is sent to fabric on epcs_rx_clk port. | Usually this must be set to 2’d1 so that the frequency of the fabric is the same as the internal side of the FWF. However variations are possible if the use of the Rx FWF synchronous enable will be employed. See FWF description for further information. | 2’d1 | |
| LCLK_EPCS_TX_CLK_SEL [1:0] | Chooses which clock is sent to fabric on epcs_tx_clk port. | 2’d1 | |||
| pcslane | LCLK_R0 | LCLK_PCS_RX_CLK_SEL [1:0] | Defines clock module’s source for pcs_rx_clk. | Must be set to 2’d3 for all applications using 8B10B function. | 2’d3 |
| LCLK_PCS_TX_CLK_SEL [1:0] | Defines clock module’s source for pcs_rx_clk. | ||||
| LCLK_RXFWF_WCLK_SEL [1:0] | Defines clock module’s source for rxfwf_wclk. | Must be consistent with L8_GEARMODE setting. | 2’d2 | ||
| LCLK_TXFWF_RCLK_SEL [1:0] | Defines clock module’s source for txfwf_rclk. | 2’d2 | |||
| LCLK_RXFWF_WCLK_PIPE | Defines whether Rx FWF is clocked by Tx side clocks or Rx side clocks. | Must be set to 1’d0 for 8B10B functionality. | 1’d0 | ||
| pcslane (continued) | LCLK_R1 | LCLK_ENA_8B10B_RX_CLK | Instructs clock module to drive 8B10B pcs_rx_clk. | Must be set to 1’d1 for 8B10B operation. | 1’d0 |
| LCLK_ENA_8B10B_RXFWF_WCLK | Instructs clock module to drive 8B10B rxfwf_wclk. | ||||
| LCLK_ENA_8B10B_TX_CLK | Instructs clock module to drive 8B10B pcs_tx_clk. | ||||
| LCLK_ENA_8B10B_TXFWF_WCLK | Instructs clock module to drive 8B10B txfwf_rclk. | ||||
| LCLK_ENA_64B6XB_RX_CLK | Instructs clock module to drive 64B6xB pcs_rx_clk. | 1’d0 | 1’d1 | ||
| LCLK_ENA_64B6XB_RX_CLK_DIV2 | Instructs clock module to drive 64B6xB pcs_rx_clk_div2. | 1’d0 | 1’d1 for 64-bit fabric 1’d0 for 32-bit fabric | ||
| LCLK_ENA_64B6XB_TX_CLK | Instructs clock module to drive 64B6xB pcs_tx_clk. | 1’d0 | 1’d1 | ||
| LCLK_ENA_64B6XB_TX_CLK_DIV2 | Instructs clock module to drive 64B6xB pcs_tx_clk_div2. | 1’b0 | 1’b1 for 64-bit fabric 1’b0 for 32-bit fabric | ||
| pma_lane | DES_CLK_CTRL | DESMODE[2:0] | Selects parallel bus width of deserializer interface. | Must select the 40-bit wide bus mode for 8b10b functionality (3’d7). | Must select the 32-bit wide bus mode for 64B6xB functionality (3’d6). |
| SER_CLK_CTRL | SERMODE[2:0] | Selects parallel bus width of serializer interface. | |||
| DES_CDR_CTRL3 | SLIP_DES_CDR_SEL | Selects source of CDR slip control. | Below setting is dependent on RX_SLIP_BIT enabled with the XCVR Configurator GUI. This has dependencies on the users fabric IP | ||
| Must be 1’d0 so that the fabric can control the symbol alignment. | Should be 1’d1 so that fabric cannot control the symbol alignment. | ||||
| SLIP_DES_CDR_EN | Optionally turns slip control OFF. | Must be set to 1’d1. | Must be set to 1’d0 | ||