2.3.2 EN, nSTRTO, PWRHLD Functionality

After a Power-On Reset (POR), when the EN pin is detected HIGH, the MCP16503 initiates the power-up sequence and transitions to Start-up mode.

Once the first power-up sequence is successfully completed, an internal status bit PSEQ_DONE is set. This bit indicates that the PMIC has completed its start-up sequence.

After PSEQ_DONE is set, the EN pin HIGH alone will no longer trigger a transition to Start-up mode. From this point onward, startup and shutdown operations can be controlled using the PWRHLD pin.

The PSEQ_DONE bit is cleared only under the following conditions:

The PSEQ_DONE bit is set when all regulators enabled during the start-up sequence have successfully ramped up, which occurs at the end of time t4, as shown in EN Power Start-up Scenario: EN Short to VIN.

nSTRTO signal is asserted LOW whenever the EN is detected to be HIGH and t1 is not expired. In case t1 is configured to be 0, nSTRTO is asserted LOW for 10  μs as long as EN pin is detected HIGH. The pin is high-Z otherwise (typically nSTRTO has an external pull-up resistor). The only exception to this input (EN) /output (nSTRTO) relationship is the so-called Automatic Wake-Up Pulse (AWKP). Please refer to section Restart Aequence After Fault During HIBERNATE: Automatic Wake-up Pulse (AWKP) Generation for the detailed timing diagram.

After the start-up sequence has been initiated, MCP16503 expects the assertion of the PWRHLD signal (Power-Hold) from the MPU to validate the sequence.

PWRHLD could be already HIGH in a typical application using a backup supply. If PWRHLD has NOT been asserted HIGH by the MPU before the completion of the start-up sequence (i.e. when nRSTO is about to be asserted high), the MCP16503 will automatically initiate a turn-off sequence.