15.4.2 HSM Parameter Configuration
(Ask a Question)To use Job Manager in the HSM flow, U-HSM parameters must be set. These parameters are stored in the user-level DEF file and automatically loaded for any new or existing Job Manager project.
U-HSM configuration data specifies:
- IP address of the U-HSM server
- U-HSM UUID assigned by Microchip
- U-HSM Master Key UUID
- Default location of the keyset repository (see the Libero SoC Design Flow User Guide )
- M-HSM UUID assigned by Microchip
The set_hsm_params
Tcl command is used to configure HSM. See 15.4.8 Tcl Interface for details.