8.1.4.6 Log Window

The Log window displays the following:
  • Informational messages such as the location and name of the files used to display the view.
  • Any syntax errors in the HDL file if the HDL file is opened with the Open File Location option (right click design object > Open File Location).
Important: The Log window displays by default when the Netlist Viewer opens. Hiding the Log window will leave more display area for the Canvas view. To get a larger display area for the Canvas view, hide the Log window (Netlist Viewer > Windows and uncheck (Show Log).
Figure 8-17. Log Window