20.2.6 Programming the Application Bitstream

To program the application bit stream:

  1. Use Libero SoC or FlashProExpress to program the FPGA fabric array, sNVM, eNVM and any security settings.
  2. Use Libero SoC to program any eNVM client.
Note: SoftConsole must be used to program the Boot mode.
Alternatively, you can also perform the following steps:
  1. Use SoftConsole to program the eNVM with the First Stage Boot image.
    1. Select the project you want programmed to eNVM in SoftConsole’s Project Explorer pane.
    2. Click the PolarFire SoC Boot Mode 1 external tool.
Programming progress messages appear in the Console.

For more information, see PolarFire SoC Software Development and Tool Flow User Guide .