21.5.6 hdl_core_extract_ports_and_parameters
(Ask a Question)Description
This Tcl command automatically extracts ports and generic parameters from an HDL core module description.
The command will fail if the module name is not specified or is incorrect.
hdl_core_extract_ports_and_parameters \
-hdl_core_name { hdl_core_name }Arguments
| Parameter | Type | Description | 
|---|---|---|
hdl_core_name  | string  | Specifies the HDL core name from which you want to extract signal names and generic parameters. This is a mandatory argument.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Required parameter 'hdl_core_name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'hdl_core_extract_ports_and_parameters -hdl_core_name "hdl_core_name"'  | 
Supported Families
| PolarFire® | 
| PolarFire SoC | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
| RTG4™ | 
Example
The following example automatically extracts ports and parameters from an "test_hdl_core" HDL core module description:
hdl_core_extract_ports_and_params -hdl_core_name {test_hdl_core}See Also
hdl_core_delete_parameters