Adding a Macro
(Ask a Question)A macro is a basic low-level design object from the Macro Library in the Catalog. Right click a macro in the Design Tree and select Load Selection to add a macro. Adding a macro adds the instance with its connected nets to the view. The connected nets are always dashed yellow lines, even if they are not connected to any logic outside the view. Double clicking the net adds connections (if any) and turns the net from a dashed line to a solid line. A solid line for a net indicates that it is a user-added net.