1.2 PolarFire® SoC MSS Configurator v2025.1 Welcome Page
(Ask a Question)The PolarFire® SoC Microprocessor Subsystem (MSS) Configurator is a software tool to configure the PolarFire SoC microprocessor subsystem. The MSS configuration is imported by the Libero® SoC Design Suite in the FPGA design flow and SoftConsole in the embedded design flow.
What's New in PolarFire SoC Standalone MSS Configurator v2025.1
(Ask a Question)MSS_DDR 16-bit width with ECC enabled: Updated MSS Configurator component XML to
                enable correct ECC byte-lane and ensure successful DDR memory training.
        Note: MPFS HAL versions later than
                    v2.3.105 are required from the PolarFire SoC GitHub organization to use this
                    change.
Getting Started
(Ask a Question)- To start configuring a new MSS subsystem, select New from the project menu.
 - To open an existing configuration file (.cfg), select Open from the project menu.
 - To save the current configuration of the MSS subsystem, select Save or Save As from the project menu.
 - To generate the MSS component file (.cxz), select Generate from the project menu after configuring the MSS subsystem. The MSS component file can be imported into Libero SoC tool. MSS configuration (.cfg) file will also be generated along with XML file.
 - To close the current
                    configuration file (.cfg) select
                        Close from the project menu. Important: The current configuration file needs to be closed before starting a new configuration.
 
Working Modes
(Ask a Question)- Batch Mode: PolarFire SoC MSS Configurator tool can be executed in batch mode. For example:
pfsoc_mss -GENERATE -CONFIGURATION_FILE:<absolute or relative path for configuration file name (.cfg)> -OUTPUT_DIR:<absolute or relative path for output directory> -EXPORT_HDL:<true/false> -LOGFILE:<absolute or relative path for logfile file name>Important: The argument-GENERATEmust be specified to generate the MSS component and the XML file in batch mode.-EXPORT_HDLand-LOGFILEare optional arguments. - GUI Mode:
                    PolarFire SoC MSS Configurator tool can be opened in the graphical user
                    interface (GUI) mode for a particular configuration file. For
                    example:
pfsoc_mss -CONFIGURATION_FILE:<absolute or relative path for configuration file name (.cfg)> 
More Information
(Ask a Question)Libero SoC Design Suite Help Documentation
- For Release Notes, Known issues, and Limitations, see Libero SoC Design Suite Release Notes.
 - For the new Libero SoC Design Suite Help documentation, which provides robust search and navigation as well as HTML-based content, see Libero SoC Design Suite Help Documentation.
 - Click here to download the latest Libero SoC Design Suite Help documentation (in HTML file format) for offline reference. Extract the contents of the 
.ziparchive and open theindex.htmlfile in a web browser of your choice. 
FPGA Design Resources
Click the following links to explore our other FPGA design resources:
Licensing
Libero software and DirectC license orders are now supported through Microchip purchasing portal. Most of the software tools and FPGA IP cores are freely available but some high-value IP cores and resources needed to work with high-density FPGAs require paid licenses. For more information, see Licensing.