1.3 What’s New in SmartHLS™ 2025.1
(Ask a Question)Release Date: May 2025
Software Features and Enhancements
- Upgraded Compilation Environment
 - 
            
- The core compiler framework has been upgraded from Clang/LLVM 14.0.6 to 15.0.7.
 - The software simulation compiler has been upgraded from GNU GCC 5.4 to 8.5.
 - In SmartHLS 2024.2 and earlier, the
                C++ standard used for design compilation was preset to C++11. Now, it is
                customizable by setting the new 
CXX_STANDARDMakefile variable , with the default set to 14 (for C++14). For example, users can compile their designs in C++17 mode by addingCXX_STANDARD=17to the HLS Makefile. 
 - Improved Multiplication Synthesis
 - The process of multiplication splitting, which decomposes and maps wide multiplication operations to target Math blocks, has been improved. This improvement involves adopting a refined multiplication characterization method that ensures more accurate resource and performance estimates for all supported multiplication modes on the target device. This facilitates the derivation of improved circuitry.
 - Improved Pointer Casting Support
 - 
            
- SmartHLS now supports type casting of pointers that point to arrays of primitive
                data types, whether passed as input arguments or declared locally within a function,
                provided that the alignment rules specified in the C/C++ standard are not violated.
                An example is shown
                below:
void dut( uint8_t in_8[N] ) { uint8_t local_8[N]; uint32_t *pin8_32 = (uint32_t *)in_8; uint32_t *plocal8_32 = (uint32_t *)local_8; }
 - Support type casting between primitive data typed array/pointer and the size
                equivalent HLS arbitrary precision data typed array/pointer. For more information,
                see Libraries. An example is shown
                below:
uint8_t d_u8[N]; hls::ap_uint<8> *p_u8 = (hls::ap_uint<8> *)d_u8;
 
 - SmartHLS now supports type casting of pointers that point to arrays of primitive
                data types, whether passed as input arguments or declared locally within a function,
                provided that the alignment rules specified in the C/C++ standard are not violated.
                An example is shown
                below:
 - API Update in Streaming Library
 - 
            
full()should only be used in design code that generates output data to the corresponding FIFO.empty()should only be used in design code that consumes input data from the corresponding FIFO.- To assist debugging in software simulation, a FIFO can now be identified by
                assigning a user-defined name using the new 
setName()API. 
 - Improved HLS Pipeline Result Reports
 - 
            
- The resource constraint report for designs utilizing the HLS utility library, such
                as the arbitrary precision library, has been enhanced. In SmartHLS 2024.2 or earlier
                version, the report would attribute resource consumption to the HLS utility code,
                which could obscure the actual source of resource usage within the user's design.
                For example, the table below reports resource constraint of a design that uses the
                arbitrary precision data types in SmartHLS 2024.2. The locations of the
                  
loadoperations are pointing to the library code that implements the arbitrary precision data type functionality; however, it does not help locating the source in the user code.+-------------------------------------+------------------------------------------------------------------------------------------------------+---------------------+ | Operation | Location | Competing Use Count | +-------------------------------------+------------------------------------------------------------------------------------------------------+---------------------+ | 'load' (5b) operation for array 'A' | line 348 of C:/Microchip/Libero_SoC_v2024.2/SmartHLS-2024.2/SmartHLS/smarthls-library/hls/ap_int.hpp | 1 | | 'load' (5b) operation for array 'A' | line 348 of C:/Microchip/Libero_SoC_v2024.2/SmartHLS-2024.2/SmartHLS/smarthls-library/hls/ap_int.hpp | 2 | | 'load' (5b) operation for array 'A' | line 348 of C:/Microchip/Libero_SoC_v2024.2/SmartHLS-2024.2/SmartHLS/smarthls-library/hls/ap_int.hpp | 3 | +-------------------------------------+------------------------------------------------------------------------------------------------------+---------------------+ | | Total # of Competing Uses | 3 | +-------------------------------------+------------------------------------------------------------------------------------------------------+---------------------+With the report improvement in this release, the same table now looks like the following.+-------------------------------------+---------------------------+---------------------+ | Operation | Location | Competing Use Count | +-------------------------------------+---------------------------+---------------------+ | 'load' (5b) operation for array 'A' | line 12 of loop.cpp | 1 | | 'load' (5b) operation for array 'A' | line 12 of loop.cpp | 2 | | 'load' (5b) operation for array 'A' | line 12 of loop.cpp | 3 | +-------------------------------------+---------------------------+---------------------+ | | Total # of Competing Uses | 3 | +-------------------------------------+---------------------------+---------------------+ - HLS pipeline reports are enhanced to handle non-constant but bounded trip count
                and latency. Here is an example of the
                report.
+-------------------------------------------------------------------------------------------+ | Function: top takes 0 - 22 cycles | +----------+--------------------------+------------+-------------------+----+---------------+ | Loop | Location In Source | Trip Count | Iteration Latency | II | Total Latency | +----------+--------------------------+------------+-------------------+----+---------------+ | for_loop | line 16 of loop_test.cpp | 0 - 16 | 1 | 1 | 0 - 16 | +----------+--------------------------+------------+-------------------+----+---------------+ 
 - The resource constraint report for designs utilizing the HLS utility library, such
                as the arbitrary precision library, has been enhanced. In SmartHLS 2024.2 or earlier
                version, the report would attribute resource consumption to the HLS utility code,
                which could obscure the actual source of resource usage within the user's design.
                For example, the table below reports resource constraint of a design that uses the
                arbitrary precision data types in SmartHLS 2024.2. The locations of the
                  
 - Enhanced Board Support
 - Soft-MiV RV32 can now run on-board using SoC Flow. For more information, see Automated SOC Flow (Beta Version).
 
Resolved Issues
The following issues have been resolved in the 2025.1 version:
    - Fixed the 
invalid command name "work.configure"error message generated from co-simulation with waveform. - Fixed incorrect design output caused by typecasting of local array pointers.
 - Fixed co-simulation crash caused by non-flushed output stream buffers during software simulation. The problem appeared on Windows platforms only.
 - Fixed crash caused by LLVM linker merging user 
structtypes that are isomorphic to SmartHLS's arbitrary data types together. - Errored out input designs that contain variable-sized storage allocation.
 - Generated warning when memory I/O operation with access size wider than target data bus is found in the design.
 - Allowed conversion between primitive array data type pointers and the size-equivalent
              
ap_int/ap_uintarray pointers through simple pointer casting in both hardware synthesis and software simulation. - Fixed bugs in latency estimation of pipelined loops and enhanced the accuracy and comprehensiveness of the reports.
 - Fixed crash caused by pass-by-reference argument in HLS threaded function.
 - Fixed crash that happened when a 
float-typed variable is used as an induction variable in a loop. - Fixed co-simulation bug caused by same-name functions existing at different scopes of the input design.
 - Fixed a bug in calling a stack of dataflow functions multiple times.
 - Errored out input designs that contain array of pointers as top-level function argument.
 - Enhanced '
[HLS pragma] ignored' warning messages with source code location. - Fixed various IDE problems.
 - Ceased the generation of unnecessary Verilog memory initialization files.