21.7.1 mss_configure_envm
(Ask a Question)This command is used to specify a .cfgfile with all clients info in the ENVM core instance of the MSS component.
mss_configure_envm \
-component_name {component_name} \
-cfg_file {file_path}
        Arguments
| Parameter | Type | Description | 
|---|---|---|
| -component_name {component_name} | string | Mandatory. Name of the MSS component. | 
| -cfg_file {file_path} | string | Mandatory. Path of the configuration file(.cfg) used to configure the envm. | 
Example
mss_configure_envm -component_name {test_sb_MSS} -cfg_file{./ENVM.cfg}