17.1.6 Implementing Your Design
(Ask a Question)After completing the Synthesis and Post-Synthesis simulation in your environment, you
            must use Libero again to physically implement your design, run timing and power
            analysis, and generate your programming file.
    - Create a new Libero project for the physical implementation and layout of the design. Ensure to target the same device as in the reference project you created in Component Configuration.
 - After project creation, remove Synthesis from the tool chain in the Design Flow window (Project > Project Settings > Design Flow > Uncheck Enable Synthesis).
 - Import your post-synthesis
                        *.vm file into this project, (File >
                        Import > Synthesized Verilog Netlist (VM)).Tip: It is recommended that you create a link to this file, so that if you re-synthesize your design, Libero always uses the latest post-synthesis netlist.
- In the Design
                                Hierarchy window, note the name of the root module.
Figure 17-4. Root Module in Design Hierarchy  
 - In the Design
                                Hierarchy window, note the name of the root module.
 - Import the constraints into the
                    Libero project. Use the Constraint Manager to import
                        *.pdc/*.sdc/*.ndc constraints.
- Import I/O *.pdc constraint files (Constraints Manager > I/O Attributes > Import).
 - Import Floorplanning *.pdc constraint files (Constraints Manager > Floor Planner > Import).
 - Import *.sdc timing constraint files (Constraints Manager > Timing > Import). If your design has any of the cores listed in Overview, ensure to import the SDC file generated through derive constraint tool.
 - Import *.ndc constraint files (Constraints Manager > Netlist Attributes > Import).
 
 - Associate Constraints Files to
                    design tools.
- Open Constraint Manager (Manage Constraints > Open Manage Constraints View). Check the Place-and-Route and Timing Verification check box next to the constraint file to establish constraint file and tool association. Associate the *.pdc constraint to Place-and-Route and the *.sdc to both Place-and-Route and Timing Verification. Associate the *.ndc file to Compile Netlist.
 
Tip: If Place and Route fails with this *.sdc constraint file, then import this same *.sdc file to synthesis and re-run synthesis. - Click Compile Netlist and then Place and Route to complete the layout step.
 - The Configure Design
                    Initialization Data and Memories tool allows you to initialize design blocks,
                    such as LSRAM, µSRAM, XCVR (transceivers), and PCIe using data stored in
                    nonvolatile µPROM, sNVM, or external SPI Flash storage memory. The tool has the
                    following tabs for defining the specification of the design initialization
                    sequence, the specification of the initialization clients, user data clients.
- Design Initialization tab
 - µPROM tab
 - sNVM tab
 - SPI Flash tab
 - Fabric RAMs tab
 
Use the tabs in the tool to configure the design initialization data and memories.
Figure 17-5. Design Initialization Data and Memories After completing the configuration, perform the following steps to program the initialization data:- Generate initialization clients
 - Generate or export the bitstream
 - Program the device
 
For detailed information on how to use this tool, see Libero SoC Design Flow User Guide . For more information on the Tcl commands used to configure various tabs in the tool and specify memory configuration files (*.cfg), see Tcl Commands Reference Guide .
 - Generate a Programming File from this project and use it to program your FPGA.