3.6.3.8 SHLS-18
(Ask a Question)Message
Warning: (SHLS-18) User specified field partitioning for '{variable}' on {location} is ignored because it does not have a struct type.
This message indicates that the pragma '#pragma HLS memory partition variable
(<Variable>) type(struct_fields) ' has been misused on a variable that is not of
struct type, and will therefore be ignored.
/***************************************************************** * This example is expected to result in * - Code : SHLS-18 * - Type : Warning * - Cause : Memory partitioning by struct field is requested * to apply on a variable that is not of a struct type. *****************************************************************/ #pragma HLS memory partition variable(array) type(struct_fields) int array[10]; void DUT() { #pragma HLS function top for (int i = 0; i < 10; i++) { array[i] *= 2; } }
Related to: Memory Partitioning