DRV_ENC28J60_Process Function
C
TCPIP_MAC_RES DRV_ENC28J60_Process(DRV_HANDLE hMac); Returns
TCPIP_MAC_RES_TYPE_ERR - if the hMac is invalid
TCPIP_MAC_RES_OP_ERR - if the hMac is valid
Description
ENC28J60 Process This function does additional processing that is not done inside the tasks function.
Remarks
This function does nothing in the first release.
Preconditions
The client had to be successfully opened with DRV_ENC28J60_Open.
Parameters
| Parameters | Description |
|---|---|
| hMac | the successfully opened handle |