DRV_ENC28J60_PacketRx Function
C
TCPIP_MAC_PACKET* DRV_ENC28J60_PacketRx(DRV_HANDLE hMac, TCPIP_MAC_RES* pRes, const TCPIP_MAC_PACKET_RX_STAT** ppPktStat); Returns
Pointer to a valid packet - if successful
NULL - if unsuccessful
Description
ENC28J60 Receive Packet This function retrieves a packet from the driver. The packet needs to be acknowledged with the linked acknowledge function so it can be reused.
Remarks
ppPktStat is ignored in the first release.
Preconditions
The client had to be successfully opened with DRV_ENC28J60_Open.
Parameters
| Parameters | Description |
|---|---|
| hMac | the successfully opened handle |
| pRes | the result of the operation |
| ppPktStat | pointer to the receive statistics |