gethostname Function
C
int gethostname(
char* name,
int namelen
);
Description
This function returns the standard host name of the system which is calling this function. The returned name is null-terminated.
Preconditions
None.
Parameters
| Parameters | Description |
|---|---|
| name | Pointer to a buffer that receives the local host name. |
| namelen | Size of the name array. |
Returns
0 - The function was successful.
SOCKET_ERROR (-1) - Name is too short to hold the host name or any other error occurs. errno is set accordingly and *name will be unmodified and no null terminator will be generated.
Remarks
The function returns the host name as set on the default network interface.