socket Function
C
SOCKET socket(
int af,
int type,
int protocol
);
Description
This function creates a new BSD socket for the Microchip TCP/IP stack. The return socket descriptor is used for the subsequent BSD operations.
Preconditions
The BerkeleySocketInit() function should be called.
Parameters
| Parameters | Description |
|---|---|
| af | Address family - AF_INET for IPv4 and AF_INET6 for IPv6. |
| type | Socket type SOCK_DGRAM or SOCK_STREAM. |
| protocol | IP protocol IPPROTO_UDP or IPPROTO_TCP. |
Returns
If the function is successful, a new socket descriptor is returned.
A return value of SOCKET_ERROR (-1) indicates an error and errno is set accordingly.
Remarks
None.