TCPIP_BSD_PresSocket Function
C
int TCPIP_BSD_PresSocket(
SOCKET s
);
Description
The function returns the NET_PRES socket number associated with the BSD socket. Using this call, the caller can access the NET_PRES API.
Preconditions
The socket() function should have been called.
Parameters
| Parameters | Description |
|---|---|
| s | Socket descriptor returned from a previous call to socket(). |
Returns
>= 0 - If function is successful. Value refers to socket number.
-1 - No such socket exists and errno is set to EBADF.
Remarks
This function works for both TCP and UDP sockets.
The NET_PRES UDP sockets are created after a call to bind() (server sockets) or connect() (client sockets). The NET_PRES TCP sockets are created after a call to listen() (server sockets) or connect() (client sockets). Calling the TCPIP_BSD_PresSocket before the sockets are created will return an INVALID_SOCKET.
The BSD module uses the NET_PRES layer for supporting encrypted connections. This function returns the NET_PRES socket used for the connection.