TCPIP_TELNET_AUTH_HANDLER Type
C
typedef bool (* TCPIP_TELNET_AUTH_HANDLER)(const char* user, const char* password, const TCPIP_TELNET_CONN_INFO* pInfo, const void* hParam);
Description
Telnet authentication callback.
Pointer to a function that will be called by the telnet module when a login operation is ongoing and user authentication needs to be performed.
Preconditions
None.
Members
| Members | Description |
|---|---|
| user | The user name entered as part of the login process. |
| password | The password entered as part of the login process. |
| pInfo | Pointer to a TCPIP_TELNET_CONN_INFO carrying specific connection information to help in the authentication process. |
| hParam | Parameter that was passed at the time of the handler registration. |
Returns
True - If the authentication is successful and the telnet connection should be allowed.
False - If the authentication failed and the connection should be aborted.
Remarks
The handler is called in the telnet context. The handler should be kept as short as possible as it shouldn't block.
This is the PREFERRED method of authenticating the telnet connection.
Until the moment the authentication handler is registered any login attempts will fail.
The pInfo will be NULL if the telnet module is initialized with TCPIP_TELNET_AUTHENTICATION_INFO == true.