TCPIP_TELNET_ConnectionInfoGet Function
C
bool TCPIP_TELNET_ConnectionInfoGet(
uint16_t connIx,
TCPIP_TELNET_CONN_INFO* pInfo
);
Description
This function gets information about a telnet connection.
Preconditions
The Telnet module should have been initialized.
Parameters
| Parameters | Description |
|---|---|
| connIx | Index of the connection to get the info for. Valid range is . |
| pInfo | Pointer to a TCPIP_TELNET_CONN_INFO to be filled with connection data Could be NULL if not needed. |
Returns
True - If the connIx is a valid telnet connection number.
False - Otherwise.
Remarks
None.