TCPIP_TELNET_AuthenticationRegister Function
C
TCPIP_TELNET_HANDLE TCPIP_TELNET_AuthenticationRegister(
TCPIP_TELNET_AUTH_HANDLER authHandler,
const void* handlerParam
);
Description
This function registers a new authentication handler. telnet module will call the handler when an user tries to login and needs to be authenticated.
Preconditions
Telnet properly initialized.
Parameters
| Parameters | Description |
|---|---|
| authHandler | The handler which will be called for authentication. |
| handlerParam | Handler parameter that will be called with the handler unused by telnet. |
Returns
A valid TCPIP_TELNET_HANDLE - If the operation succeeded.
NULL - If the operation failed.
Remarks
Currently only one authentication handler is supported by the telnet module. The call will fail if a handler is already registered. Use TCPIP_TELNET_AuthenticationDeregister() first.
This is the PREFERRED authentication method! If there's no registrated handler, any login attempt will fail.
The build should have TCPIP_TELNET_OBSOLETE_AUTHENTICATION == false.
Example
TCPIP_TELNET_HANDLE authHandle = TCPIP_TELNET_AuthenticationRegister( myAuthHandler, myParam );