TCPIP_DNSS_AddressCntGet Function
C
TCPIP_DNSS_RESULT TCPIP_DNSS_AddressCntGet(
int index,
uint8_t * hostName,
uint8_t * ipCount
);
Description
This function is used to get the number of IPv4 and IPv6 address entry details from hash entry table. Here input parameter is index value. Output will be the hostname and IP address count. IP address count is the summation of both IPv4 and IPv6 address.
Preconditions
DNSServerInit() should be called.
Parameters
| Parameters | Description |
|---|---|
| hostName | Get DNS host name. |
| ipCount | Get the number of IPv4 or IPv6 Server address. |
| index | Server count details per index value. |
Returns
TCPIP_DNSS_RES_OK - If entry remove is successful.
TCPIP_DNSS_RES_NO_ENTRY - No such entry is present.
TCPIP_DNSS_RES_MEMORY_FAIL - No Memory is present for IPv4 or IPv6 address type.
Remarks
None.