TCPIP_STACK_PacketHandlerRegister Function
C
TCPIP_STACK_PROCESS_HANDLE TCPIP_STACK_PacketHandlerRegister(
TCPIP_NET_HANDLE hNet,
TCPIP_STACK_PACKET_HANDLER pktHandler,
const void* handlerParam
);
Description
This function registers a new packet processing handler. The caller can use the handler to be notified of incoming packets and given a chance to examine/process them.
Preconditions
The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY. The network interface should be up and running.
Parameters
Parameters | Description |
---|---|
hNet | Network handle. |
pktHandle | The packet handler which will be called for an incoming packet. |
handlerParam | Packet handler parameter. |
Returns
A valid TCPIP_STACK_PROCESS_HANDLE - If the operation succeeded.
NULL - If the operation failed.
Remarks
Currently only one packet handler is supported per interface. The call will fail if a handler is already registered. Use TCPIP_STACK_PacketHandlerDeregister() first.
Exists only if TCPIP_STACK_EXTERN_PACKET_PROCESS is true.
Example
TCPIP_STACK_PROCESS_HANDLE pktHandle = TCPIP_STACK_PacketHandlerRegister( hNet, myPktHandler, myParam );