TCPIP_STACK_NetMulticastGet Function

C

TCPIP_NET_HANDLE TCPIP_STACK_NetMulticastGet();

Description

This function returns the current default multicast network interface in the TCP/IP stack. This is the interface on which IGMP and multicast packets will be transmitted when a default interface is specified.

Preconditions

The TCP/IP stack should have been initialized by TCPIP_STACK_Initialize() and the TCPIP_STACK_Status() returned SYS_STATUS_READY.

Returns

  • The fault multicast network interface.

Remarks

This function is intended for a TCP/IP stack implementing IGMP.