TCPIP_Helper_StringToIPv6Address Function
C
bool TCPIP_Helper_StringToIPv6Address(
const char * str,
IPV6_ADDR * addr
);
Description
This function parses the text representation of an IPv6 address to an IPV6_ADDR struct. The output result is big-endian.
Preconditions
addr - valid pointer to an IPV6 address.
Parameters
Parameters | Description |
---|---|
str | Pointer to an RFC3513, Section 2.2 text representation of an IPv6 address. |
Returns
If str == NULL or strlen(str) == 0, the result will be address 0.
Remarks
1111:2222:3333:4444:5555:6666:AAAA:FFFF 1111:2222::FFFF 1111:2222:3333:4444:5555:6666:192.168.1.20 addr - Pointer to IPV6_ADDR in which to store the result.