TCPIP_STACK_Status Function
C
SYS_STATUS TCPIP_STACK_Status(
SYS_MODULE_OBJ object
);
Description
This function provides the current status of the TCPIP stack moodule.
Preconditions
The TCPIP_STACK_Initialize() function must have been called before calling this function.
Parameters
Parameters | Description |
---|---|
object | Object handle, returned from TCPIP_STACK_Initialize(). |
Returns
SYS_STATUS_READY - Indicates that any previous initialization operation for the stack has completed.
SYS_STATUS_BUSY - Indicates that a previous initialization operation for the stack has not yet completed.
SYS_STATUS_ERROR - Indicates that the initialization operation has failed and the stack is in an error state.
Remarks
After calling TCPIP_STACK_Initialize(), the stack will continue its initialization process in the TCPIP_STACK_Task() routine. This may take some time. The stack is ready to use only when the TCPIP_STACK_Status() returned SYS_STATUS_READY.