DRV_GMAC_RxFilterHashTableEntrySet Function
C
TCPIP_MAC_RES DRV_GMAC_RxFilterHashTableEntrySet(DRV_HANDLE hMac, const TCPIP_MAC_ADDR* DestMACAddr);
Returns
TCPIP_MAC_RES_OK if success
a TCPIP_MAC_RES error value if failed
Description
This function sets the MAC hash table filtering to allow packets sent to DestMACAddr to be received. It calculates a CRC-32 using polynomial 0x4C11DB7 over the 6 byte MAC address and then, using bits 28:23 of the CRC, will set the appropriate bits in the hash table filter registers ( ETHHT0-ETHHT1). The function will enable/disable the Hash Table receive filter if needed.
Remarks
Sets the appropriate bit in the ETHHT0/1 registers to allow packets sent to DestMACAddr to be received and enabled the Hash Table receive filter.
There is no way to individually remove destination MAC addresses from the hash table since it is possible to have a hash collision and therefore multiple MAC addresses relying on the same hash table bit.
A workaround is to have the stack store each enabled MAC address and to perform the comparison at run time.
A call to DRV_GMAC_RxFilterHashTableEntrySet() using a 00-00-00-00-00-00 destination MAC address, which will clear the entire hash table and disable the hash table filter. This will allow the receive of all packets, regardless of their destination
Preconditions
DRV_GMAC_Initialize() should have been called. DRV_GMAC_Open() should have been called to obtain a valid handle.