DRV_GMAC_RegisterStatisticsGet Function
C
TCPIP_MAC_RES DRV_GMAC_RegisterStatisticsGet(DRV_HANDLE hMac, TCPIP_MAC_STATISTICS_REG_ENTRY* pRegEntries, int nEntries, int* pHwEntries);
Returns
TCPIP_MAC_RES_OK if all processing went on OK.
TCPIP_MAC_RES_OP_ERR error code if function not supported by the driver.
Description
This function will get the current value of the statistic registers of the associated MAC controller.
Remarks
The reported values are info only and change dynamically.
Preconditions
DRV_GMAC_Initialize() should have been called. DRV_GMAC_Open() should have been called to obtain a valid handle.