DRV_GMAC_EventPendingGet Function
C
TCPIP_MAC_EVENT DRV_GMAC_EventPendingGet(DRV_HANDLE hMac);
Returns
The currently stack pending events.
Description
This function returns the currently pending Ethernet MAC events. Multiple events will be ORed together as they accumulate. The stack should perform processing whenever a transmission related event (TCPIP_MAC_EV_RX_PKTPEND, TCPIP_MAC_EV_TX_DONE) is present. The other, non critical events, may not be managed by the stack and passed to an user. They will have to be eventually acknowledged if re-enabling is needed.
Remarks
This is the preferred method to get the current pending MAC events. The stack maintains a proper image of the events from their occurrence to their acknowledgment.
Even with a notification handler in place it's better to use this function to get the current pending events rather than using the events passed by the notification handler which could be stale.
The events are persistent. They shouldn't be re-enabled unless they have been processed and the condition that generated them was removed. Re-enabling them immediately without proper processing will have dramatic effects on system performance.
The returned value is just a momentary value. The pending events can change any time.
Preconditions
DRV_GMAC_Initialize() should have been called. DRV_GMAC_Open() should have been called to obtain a valid handle.
Example
TCPIP_MAC_EVENT currEvents = DRV_GMAC_EventPendingGet( hMac);