3.7 LEDs
The on-board LEDs are categorized into two types:
The following table provides details about the list of LEDs that the user can turn ON or OFF while using the connected GPIO pins:
| Pin on the WFI32E01 Module | Description | Function |
|---|---|---|
| RPK1/RK1 | RF front-end control/remappable peripheral/PORTK digital I/O | Red LED (D202) |
| RPK3/RK3 | RF front-end control/remappable peripheral/PORTK digital I/O | Green LED (D204) |