7.2 Host MCU Interface
An external MCU controls the IS20xxS SoC using the UART command set. The following figure illustrates the UART interface between the IS20xxS SoC and an external MCU.
The MCU controls the IS20xxS SoC over the UART interface and wakes up the SoC using the PWR pin. The MCU function wakes up by connecting to the P0_0 pin of the IS20xxS.
Refer to the IS200x/IS201x/IS202x UART Command SOP document for a list of functions that the IS20xxS SoC supports and how to use the IS20XXS_UI tool to set up the system using the UART command.
Note: The IS200x/IS201x/IS202x UART Command
SOP document is available for download from the Microchip website at IS200x/IS201x/IS202x UART Command SOP.