4.2 Determining the ATSAMC21-XPRO Virtual COM Port Number
The system software consists of a CARS kit PC evaluation utility, which runs on a host PC and communicates with the ATSAMC21-XPRO board via the virtual COM port. Install the USB driver (Windows 10 and later) to support the ATSAMC21-XPRO virtual COM port via a USB connection (see XPRO USB Driver Installation).
Perform the following steps for determining the ATSAMC21-XPRO virtual COM port number:
- Connect the micro-USB plug to the USB connector on the ATSAMC21-XPRO board.
- Connect the other end of the USB cable to an open USB port on the PC. Open the Windows Device Manager on the PC.
- Expand the “Ports (COM & LPT)” menu, then
note the COM port assigned to the “EDBG Virtual COM Port”. In this example, COM17 is
used while connecting the CARS kit evaluation utility program to the ATSAMC21-XPRO
board.
Figure 4-1. Virtual COM Port Assignment
Note: Always ensure that the adapter cable
and the USB cable are unplugged prior to inserting or removing any boards within the
system.