4.6.7.4 Cmacros Option
The -mcmacros option requests that when building a
project, the command-line driver define preprocessor macros that are relevant for C
programs. This is the default action taken by the driver.
The -mno-cmacros form of this option can be used if you prefer that
C-related preprocessor macros are not defined. Those macros that relate to the device are
still defined (e.g. __16F1937 or _ROMSIZE), but any
macros that relate to the C program are suppressed (e.g. __XC8,
__OPTIM_FLAGS, or __SIZEOF_CHAR__). Use the
-mno-cmacros option with caution. Ensure the operation of your project
is not dependent on the presence of or value equated to these macros.