4.1.3 LPDDR1-SDRAM Initialization

The initialization sequence is generated by software. The low-power DDR1-SDRAM devices are initialized by the following sequence:

Table 4-3. LPDDR1-SDRAM Initialization
StepActionRegisterSetting
1Program the memory device typeMPDDRC_MDMD = 3 (for LPDDR1), DBW = 0 (32 bits)
2Program the shift sampling valueMPDDRC_RD_DATA_PATHSection SDRAM Controller Configuration provides values for these fields. These values depend on the DDR clock.
3Program LPDDR1-SDRAM featuresMPDDRC_CR MPDDRC_TPR0

MPDDRC_TPR 1

4Program TCR, PASR and DSMPDDRC_LPR–
5Issue a NOP command(4)MPDDRC_MRMODE = 1
6200 μs delay(1)––
7Issue a NOP command(4)MPDDRC_MRMODE = 1
8Issue an All Banks Precharge command(4)MPDDRC_MRMODE = 2
9Provide two autorefresh (CBR) cycles(4)MPDDRC_MRMODE = 4
10Issue an EMRS cycle(2)MPDDRC_MRMODE = 5
11Issue a Mode Register Set (MRS) cycle(3)MPDDRC_MRMODE = 3
12Provide a Normal Mode command(4)MPDDRC_MRMODE = 0
13Write the refresh rate in COUNT fieldMPDDRC_RTRCOUNT = Trefi/Tck
Note:
  1. To issue a delay:

    • disable interrupts;

    • compute a deadline = ROUND_INT_DIV((timer_channel_freq/1000)*count, 1000), where count is the delay in µs;
    • start a timer and wait for the timer to reach the deadline;

    • enable interrupts.
  2. To issue an Extended Mode Register Set (EMRS) cycle, after setting the MODE field to 5, read MPDDRC_MR and add a memory barrier assembler instruction just after the read. Then perform a write access to the LPDDR1-SDRAM device so that the BA[1] signal is set to 1 and BA[0] is set to 0. The address at which the write access is issued in order to acknowledge the command needs to be calculated so that the BA[1:0] signals are in the right state for an EMRS cycle.
  3. After setting the MODE field, read MPDDRC_MR and add a memory barrier assembler instruction just after the read. Perform a write access to acknowledge the command so that BA[2:0] signals are set to 0 (write at BASE_ADDRESS_DDR).
  4. After setting the MODE field, read MPDDRC_MR and add a memory barrier assembler instruction just after the read. Perform a write access at any address to acknowledge the command.


Refer to chapter "Multiport DDR-SDRAM Controller (MPDDRC)” of the SAMA5D2 Series data sheet for more information.